WedmCustomBoundaryDataBuilder Class

class NXOpen.CAM.WedmCustomBoundaryDataBuilder

Bases: NXOpen.Builder

Represents a WedmCustomBoundaryData Builder

No Creator

New in version NX6.0.0.

Properties

Property Description
InpathEventDataList Returns the inpath event data list
TabPointList Returns the tab point data list
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CreateInpathEventDataBuilder The create inpath event data builder @return inpath event data builder
CreateTabPointDataBuilder The create tab point data builder @return create tab point data builder
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

InpathEventDataList

WedmCustomBoundaryDataBuilder.InpathEventDataList

Returns the inpath event data list

-------------------------------------

Getter Method

Signature InpathEventDataList()

Returns:inpath event data list
Return type:NXOpen.CAM.InPathEventDataBuilderList

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

TabPointList

WedmCustomBoundaryDataBuilder.TabPointList

Returns the tab point data list

-------------------------------------

Getter Method

Signature TabPointList()

Returns:tab point list
Return type:NXOpen.CAM.TabPointDataBuilderList

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Method Detail

CreateInpathEventDataBuilder

WedmCustomBoundaryDataBuilder.CreateInpathEventDataBuilder

The create inpath event data builder

Signature CreateInpathEventDataBuilder()

Returns:inpath event data builder
Return type:NXOpen.CAM.InPathEventDataBuilder

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

CreateTabPointDataBuilder

WedmCustomBoundaryDataBuilder.CreateTabPointDataBuilder

The create tab point data builder

Signature CreateTabPointDataBuilder()

Returns:create tab point data builder
Return type:NXOpen.CAM.TabPointDataBuilder

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

Validate

WedmCustomBoundaryDataBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.