VerticalPositionOffsetTypes Enumeration

NXOpen.CAM.VerticalPosition.OffsetTypes is an alias for NXOpen.CAM.VerticalPositionOffsetTypes

class NXOpen.CAM.VerticalPositionOffsetTypes

Bases: object

offset options

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Distance
Distance
TeethNumber
Number of Teeth
Auto
Auto
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.