TurningToolBuilderInsertPositions Enumeration

NXOpen.CAM.TurningToolBuilder.InsertPositions is an alias for NXOpen.CAM.TurningToolBuilderInsertPositions

class NXOpen.CAM.TurningToolBuilderInsertPositions

Bases: object

the available insert positions

Enum Members

Enum Member Enum Member Description
Topside
Topside
Underside
Underside
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.