TurningToolBuilderHolderShankTypes Enumeration

NXOpen.CAM.TurningToolBuilder.HolderShankTypes is an alias for NXOpen.CAM.TurningToolBuilderHolderShankTypes

class NXOpen.CAM.TurningToolBuilderHolderShankTypes

Bases: object

the available turn holder shank types

Enum Members

Enum Member Enum Member Description
Square
Square Shank
Round
Round Shank
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.