TurnToolProbingBuilderTrackingPointTypes Enumeration

NXOpen.CAM.TurnToolProbingBuilder.TrackingPointTypes is an alias for NXOpen.CAM.TurnToolProbingBuilderTrackingPointTypes

class NXOpen.CAM.TurnToolProbingBuilderTrackingPointTypes

Bases: object

available types for tracking point

Enum Members

Enum Member Enum Member Description
Fixed
fixed
Rotate
rotate with holder
Auto
automatic
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.