TurnToolBuilderThicknessTypes Enumeration

NXOpen.CAM.TurnToolBuilder.ThicknessTypes is an alias for NXOpen.CAM.TurnToolBuilderThicknessTypes

class NXOpen.CAM.TurnToolBuilderThicknessTypes

Bases: object

the available thickness types

Enum Members

Enum Member Enum Member Description
Thickness01
Thickness: 01
ThicknessT1
Thickness: T1
Thickness02
Thickness: 02
ThicknessT2
Thickness: T2
Thickness03
Thickness: 03
ThicknessT3
Thickness: T3
Thickness04
Thickness: 04
Thickness05
Thickness: 05
Thickness06
Thickness: 06
Thickness07
Thickness: 07
Thickness09
Thickness: 09
Thickness11
Thickness: 11
Thickness12
Thickness: 12
ThicknessUserDefined
Thickness: User defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.