TurnToolBuilderInsertShapes Enumeration

NXOpen.CAM.TurnToolBuilder.InsertShapes is an alias for NXOpen.CAM.TurnToolBuilderInsertShapes

class NXOpen.CAM.TurnToolBuilderInsertShapes

Bases: object

the available insert shapes

Enum Members

Enum Member Enum Member Description
Parallelogram85
Insert shape: Parallelogram 85
Parallelogram82
Insert shape: Parallelogram 82
Diamond80
Insert shape: Diamond 80
Diamond100
Insert shape: Diamond 100
Diamond55
Insert shape: Diamond 55
Diamond75
Insert shape: Diamond 75
Hexagon
Insert shape: Hexagon
Parallelogram55
Insert shape: Parallelogram 55
Rectangle
Insert shape: Rectangle
Diamond86
Insert shape: Diamond 86
Octagon
Insert shape: Octagon
Pentagon
Insert shape: Pentagon
Round
Insert shape: Round
Square
Insert shape: Square
Triangle
Insert shape: Triangle
Diamond35
Insert shape: Diamond 35
Trigon
Insert shape: Trigon
User
Insert shape: User defined
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.