TurnToolBuilderHolderStyles Enumeration¶
NXOpen.CAM.TurnToolBuilder.HolderStyles is an alias for NXOpen.CAM.TurnToolBuilderHolderStyles
-
class
NXOpen.CAM.
TurnToolBuilderHolderStyles
¶ Bases:
object
the available turn holder style options
Enum Members
Enum Member Enum Member Description A A-StyleB B-StyleC C-StyleD D-StyleE E-StyleF F-StyleG G-StyleH H-StyleI I-StyleJ J-StyleK K-StyleL L-StyleM M-StyleN N-StyleP P-StyleQ Q-StyleR R-StyleS S-StyleT T-StyleU U-StyleV V-StyleUd User-Defined-Style-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-