TurnRoughFinishTestCutStopPositionTypes Enumeration

NXOpen.CAM.TurnRoughFinishTestCut.StopPositionTypes is an alias for NXOpen.CAM.TurnRoughFinishTestCutStopPositionTypes

class NXOpen.CAM.TurnRoughFinishTestCutStopPositionTypes

Bases: object

the test cut stop position options

Enum Members

Enum Member Enum Member Description
Automatic
Test Cut Stop Position: Automatic
Point
Test Cut Stop Position: Point
Length
Test Cut Stop Position: Length
Percent
Test Cut Stop Position: Percent of Finish Cut
SameAsFirstTestCut
Test Cut Stop Position: Same as First Test Cut
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.