TurnRoughFinishTestCutStockModeTypes Enumeration

NXOpen.CAM.TurnRoughFinishTestCut.StockModeTypes is an alias for NXOpen.CAM.TurnRoughFinishTestCutStockModeTypes

class NXOpen.CAM.TurnRoughFinishTestCutStockModeTypes

Bases: object

the test cut stock mode options

Enum Members

Enum Member Enum Member Description
Automatic
Test Cut Stock Mode: Automatic
Specify
Test Cut Stock Mode: Specify
SameAsFirstTestCut
Test Cut Stock Mode: Same as First Test Cut
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.