TurnRoughFinishTestCutSequenceTypes Enumeration¶
NXOpen.CAM.TurnRoughFinishTestCut.SequenceTypes is an alias for NXOpen.CAM.TurnRoughFinishTestCutSequenceTypes
-
class
NXOpen.CAM.
TurnRoughFinishTestCutSequenceTypes
¶ Bases:
object
the test cut sequence options
Enum Members
Enum Member Enum Member Description NotSet Test Cut Sequence: NoneTestCutAndFinish Test Cut Sequence: Test Cut and FinishTestCutOnly Test Cut Sequence: Test Cut Only-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-