TurnRoughFinishTestCutReturnMoveTypes Enumeration

NXOpen.CAM.TurnRoughFinishTestCut.ReturnMoveTypes is an alias for NXOpen.CAM.TurnRoughFinishTestCutReturnMoveTypes

class NXOpen.CAM.TurnRoughFinishTestCutReturnMoveTypes

Bases: object

the test cut return move options

Enum Members

Enum Member Enum Member Description
Direct
Test Cut Return Move: Direct
RadialAxial
Test Cut Return Move: Radial -> Axial
AxialRadial
Test Cut Return Move: Axial -> Radial
SameAsFirstTestCut
Test Cut Return Move: Same as First Test Cut
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.