TurnRoughFinishTestCutFeedInTypes Enumeration¶
NXOpen.CAM.TurnRoughFinishTestCut.FeedInTypes is an alias for NXOpen.CAM.TurnRoughFinishTestCutFeedInTypes
-
class
NXOpen.CAM.
TurnRoughFinishTestCutFeedInTypes
¶ Bases:
object
the test cut feed in options
Enum Members
Enum Member Enum Member Description NotSet Test Cut Feed In: NoneLinear Test Cut Feed In: LinearSameAsProfileEngage Test Cut Feed In: Same as Profile eEgangeSameAsFirstTestCut Test Cut Feed In: Same as First Test Cut-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-