TurnOverlap Class¶
-
class
NXOpen.CAM.
TurnOverlap
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.TurnOverlap
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns or sets the overlap distance |
Percentage | Returns or sets the overlap percentage |
Tag | Returns the Tag for this object. |
Type | Returns or sets the overlap type |
Methods¶
Enumerations¶
TurnOverlapTypes Enumeration | the overlap types |
Property Detail¶
Distance¶
-
TurnOverlap.
Distance
¶ Returns or sets the overlap distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: the overlap distance Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance(overlapDistance)
Parameters: overlapDistance (float) – the overlap distance New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Percentage¶
-
TurnOverlap.
Percentage
¶ Returns or sets the overlap percentage
-------------------------------------
Getter Method
Signature
Percentage()
Returns: the overlap percentage Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Percentage(overlapPercentage)
Parameters: overlapPercentage (float) – the overlap percentage New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
TurnOverlap.
Type
¶ Returns or sets the overlap type
-------------------------------------
Getter Method
Signature
Type()
Returns: the overlap type Return type: NXOpen.CAM.TurnOverlapTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(overlapMode)
Parameters: overlapMode ( NXOpen.CAM.TurnOverlapTypes
) – the overlap typeNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)