TurnOrientGeomBuilderLatheWorkPlaneTypes Enumeration

NXOpen.CAM.TurnOrientGeomBuilder.LatheWorkPlaneTypes is an alias for NXOpen.CAM.TurnOrientGeomBuilderLatheWorkPlaneTypes

class NXOpen.CAM.TurnOrientGeomBuilderLatheWorkPlaneTypes

Bases: object

the lathe work plane types

Enum Members

Enum Member Enum Member Description
XmYm
XM/YM plane of the MCS
ZmXm
ZM/XM plane of the MCS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.