TurnMoveToPointBuilderDirectionTypes Enumeration

NXOpen.CAM.TurnMoveToPointBuilder.DirectionTypes is an alias for NXOpen.CAM.TurnMoveToPointBuilderDirectionTypes

class NXOpen.CAM.TurnMoveToPointBuilderDirectionTypes

Bases: object

the move direction type

Enum Members

Enum Member Enum Member Description
Direct
direct
Radial
radial
Axial
axial
RadialAxial
radial axial
AxialRadial
axial radial
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.