TurnGrooveCornerControlCutSequenceTypes Enumeration

NXOpen.CAM.TurnGrooveCornerControl.CutSequenceTypes is an alias for NXOpen.CAM.TurnGrooveCornerControlCutSequenceTypes

class NXOpen.CAM.TurnGrooveCornerControlCutSequenceTypes

Bases: object

the Groove Corner Control cut sequence types

New in version NX9.0.0.

Enum Members

Enum Member Enum Member Description
CornersFirst
Groove Corner Control cut sequence is Corners First.
CornersFirstAndLast
Groove Corner Control cut sequence is Corners First and Last.
CornerWithWall
Groove Corner Control cut sequence is Corner With Wall.
CornerAfterWall
Groove Corner Control cut sequence is Corner After Wall.
CornersLast
Groove Corner Control cut sequence is Corners Last.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.