TurnFeatureGeomBuilderCutRegionSelectionModes Enumeration

NXOpen.CAM.TurnFeatureGeomBuilder.CutRegionSelectionModes is an alias for NXOpen.CAM.TurnFeatureGeomBuilderCutRegionSelectionModes

class NXOpen.CAM.TurnFeatureGeomBuilderCutRegionSelectionModes

Bases: object

the cut region selection options

Enum Members

Enum Member Enum Member Description
Automatic
Automatic cut region selection.
Manual
Manual cut region selection.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.