TurnEngageRetractBuilderTypes Enumeration¶
NXOpen.CAM.TurnEngageRetractBuilder.Types is an alias for NXOpen.CAM.TurnEngageRetractBuilderTypes
-
class
NXOpen.CAM.
TurnEngageRetractBuilderTypes
¶ Bases:
object
The engage retract type
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description AutoCircular Auto CircularAutoLinear Auto LinearDelta DeltaAngleAndDistance Angle and DistanceRelativeLinear Relative LinearFromAPoint From a PointTwoCircles Two CirclesTwoPointTangent Two Point TangentSameAsEngage Same as Engage-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-