TurnEngageRetractBuilderExtendMethods Enumeration

NXOpen.CAM.TurnEngageRetractBuilder.ExtendMethods is an alias for NXOpen.CAM.TurnEngageRetractBuilderExtendMethods

class NXOpen.CAM.TurnEngageRetractBuilderExtendMethods

Bases: object

the extend method options

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Distance
Extend by distance
ToBlank
Extend to blank
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.