TurnEngageRetractBuilderDirectEngageRetractModes Enumeration¶
NXOpen.CAM.TurnEngageRetractBuilder.DirectEngageRetractModes is an alias for NXOpen.CAM.TurnEngageRetractBuilderDirectEngageRetractModes
-
class
NXOpen.CAM.
TurnEngageRetractBuilderDirectEngageRetractModes
¶ Bases:
object
the direct engage/retact mode options
New in version NX10.0.2.
Enum Members
Enum Member Enum Member Description NotSet Direct engage/retract mode: NoneToOrFromTrimPointOnly Direct engage/retract mode: To/from trim point onlyAlways Direct engage/retract mode: Always-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-