TurnEngageRetractBuilderAutoOptions Enumeration

NXOpen.CAM.TurnEngageRetractBuilder.AutoOptions is an alias for NXOpen.CAM.TurnEngageRetractBuilderAutoOptions

class NXOpen.CAM.TurnEngageRetractBuilderAutoOptions

Bases: object

The auto engage retract options

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
UserDefinedValues
User Defined Values
AutomaticValues
Automatic Values
ClearWallsByAngleAndDistance
Clear Walls by Angle and Distance
Withdraw
Withdraw
WithdrawByDistance
Withdraw by Distance
ClearWalls
Clear Walls
ClearWallsByDistance
Clear Walls by Distance
SameAsPlungeRetract
Same as Plunge Retract
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.