TurnCutterClearance Class¶
-
class
NXOpen.CAM.
TurnCutterClearance
¶ Bases:
NXOpen.TaggedObject
Represents a
NXOpen.CAM.TurnCutterClearance
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
FirstCuttingEdge | Returns or sets the first cutting edge clearance angle |
LastCuttingEdge | Returns or sets the last cutting edge clearance angle |
Tag | Returns the Tag for this object. |
Methods¶
Property Detail¶
FirstCuttingEdge¶
-
TurnCutterClearance.
FirstCuttingEdge
¶ Returns or sets the first cutting edge clearance angle
-------------------------------------
Getter Method
Signature
FirstCuttingEdge()
Returns: the first cutting edge clearance angle Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
FirstCuttingEdge(newValue)
Parameters: newValue (float) – the first cutting edge clearance angle New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
LastCuttingEdge¶
-
TurnCutterClearance.
LastCuttingEdge
¶ Returns or sets the last cutting edge clearance angle
-------------------------------------
Getter Method
Signature
LastCuttingEdge()
Returns: the last cutting edge clearance angle Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LastCuttingEdge(newValue)
Parameters: newValue (float) – the last cutting edge clearance angle New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)