TurnCornerControlTypes Enumeration¶
NXOpen.CAM.TurnCornerControl.Types is an alias for NXOpen.CAM.TurnCornerControlTypes
-
class
NXOpen.CAM.
TurnCornerControlTypes
¶ Bases:
object
the Corner Control Types options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description RollAround Corner Control Types is Roll Around.ExtendTangents Corner Control Types is Extend Tangents.Round Corner Control Types is Round.Break Corner Control Types is Break.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-