TurnConcaveCornerControlTypes Enumeration

NXOpen.CAM.TurnConcaveCornerControl.Types is an alias for NXOpen.CAM.TurnConcaveCornerControlTypes

class NXOpen.CAM.TurnConcaveCornerControlTypes

Bases: object

the Concave Corner Control types

New in version NX6.0.2.

Enum Members

Enum Member Enum Member Description
ExtendTangents
Concave Corner Control Type is Extend.
Round
Concave Corner Control Type is Round.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.