TurnConcaveCornerControlRadiusOptions Enumeration

NXOpen.CAM.TurnConcaveCornerControl.RadiusOptions is an alias for NXOpen.CAM.TurnConcaveCornerControlRadiusOptions

class NXOpen.CAM.TurnConcaveCornerControlRadiusOptions

Bases: object

the Concave Corner Control radius options

New in version NX6.0.2.

Enum Members

Enum Member Enum Member Description
Specify
Concave Corner Control radius option is Specify.
ToolRadius
Concave Corner Control radius option is Tool Radius.
AddToToolRadius
Concave Corner Control radius option is Add to Tool Radius.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.