TurnAvoidanceReturnBuilderReturnPointModes Enumeration

NXOpen.CAM.TurnAvoidanceReturnBuilder.ReturnPointModes is an alias for NXOpen.CAM.TurnAvoidanceReturnBuilderReturnPointModes

class NXOpen.CAM.TurnAvoidanceReturnBuilderReturnPointModes

Bases: object

The return point mode options

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Point
Point is defined by point.
DeltaAngleDistance
Point is defined by angle and distance.
DeltaVectorDistance
Point is defined by vector and distance.
DeltaMove
Point is defined by delta move (X and Y coordinate).
SameAsStart
Point is locked start point.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.