TurnAvoidanceGohomeBuilderGohomePointModes Enumeration

NXOpen.CAM.TurnAvoidanceGohomeBuilder.GohomePointModes is an alias for NXOpen.CAM.TurnAvoidanceGohomeBuilderGohomePointModes

class NXOpen.CAM.TurnAvoidanceGohomeBuilderGohomePointModes

Bases: object

The gohome point mode options

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Point
Point is defined by point.
SameAsFrom
Point is locked to from point.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.