Properties¶
Property | Description |
---|---|
GohomePoint | Returns or sets the gohome point |
GohomePointMode | Returns or sets the gohome point mode |
GohomePointMotionType | Returns or sets the gohome point motion type |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
TurnAvoidanceGohomeBuilderGohomePointModes Enumeration | The gohome point mode options |
TurnAvoidanceGohomeBuilderGohomePointMotionTypes Enumeration | The gohome point motion type options |
Property Detail¶
GohomePoint¶
-
TurnAvoidanceGohomeBuilder.
GohomePoint
¶ Returns or sets the gohome point
-------------------------------------
Getter Method
Signature
GohomePoint()
Returns: the gohome point value Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GohomePoint(gohomePoint)
Parameters: gohomePoint ( NXOpen.Point
) – the gohome point valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
GohomePointMode¶
-
TurnAvoidanceGohomeBuilder.
GohomePointMode
¶ Returns or sets the gohome point mode
-------------------------------------
Getter Method
Signature
GohomePointMode()
Returns: the gohome point mode value Return type: NXOpen.CAM.TurnAvoidanceGohomeBuilderGohomePointModes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GohomePointMode(gohomePointMode)
Parameters: gohomePointMode ( NXOpen.CAM.TurnAvoidanceGohomeBuilderGohomePointModes
) – the gohome point mode valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
GohomePointMotionType¶
-
TurnAvoidanceGohomeBuilder.
GohomePointMotionType
¶ Returns or sets the gohome point motion type
-------------------------------------
Getter Method
Signature
GohomePointMotionType()
Returns: the gohome point motion type value Return type: NXOpen.CAM.TurnAvoidanceGohomeBuilderGohomePointMotionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
GohomePointMotionType(gohomePointMotionType)
Parameters: gohomePointMotionType ( NXOpen.CAM.TurnAvoidanceGohomeBuilderGohomePointMotionTypes
) – the gohome point motion type valueNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)