TurnAvoidanceFromBuilder Class

class NXOpen.CAM.TurnAvoidanceFromBuilder

Bases: NXOpen.TaggedObject

Represents an avoidance from Builder

New in version NX6.0.0.

Properties

Property Description
FromPoint Returns or sets the from point
FromPointMode Returns or sets the from point mode
Tag Returns the Tag for this object.

Methods

Enumerations

TurnAvoidanceFromBuilderFromPointModes Enumeration The from point mode options

Property Detail

FromPoint

TurnAvoidanceFromBuilder.FromPoint

Returns or sets the from point

-------------------------------------

Getter Method

Signature FromPoint()

Returns:the from point value
Return type:NXOpen.Point

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FromPoint(fromPoint)

Parameters:fromPoint (NXOpen.Point) – the from point value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)

FromPointMode

TurnAvoidanceFromBuilder.FromPointMode

Returns or sets the from point mode

-------------------------------------

Getter Method

Signature FromPointMode()

Returns:the from point mode value
Return type:NXOpen.CAM.TurnAvoidanceFromBuilderFromPointModes

New in version NX6.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature FromPointMode(fromPointMode)

Parameters:fromPointMode (NXOpen.CAM.TurnAvoidanceFromBuilderFromPointModes) – the from point mode value

New in version NX6.0.0.

License requirements: cam_base (“CAM BASE”)