TrimPointRampAngleOptions Enumeration¶
NXOpen.CAM.TrimPoint.RampAngleOptions is an alias for NXOpen.CAM.TrimPointRampAngleOptions
-
class
NXOpen.CAM.
TrimPointRampAngleOptions
¶ Bases:
object
The trim point ramp angle options
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description NotSet no ramp angle.Aligned Ramp angle is aligned to angle.Vector Ramp angle is defined by a vector.Angle Ramp angle is defined by a value.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-