TrimPlaneContent Enumeration

NXOpen.CAM.TrimPlane.Content is an alias for NXOpen.CAM.TrimPlaneContent

class NXOpen.CAM.TrimPlaneContent

Bases: object

The content options

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
Radial
radial
Axial
axial.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.