TrackpointBuilder Class

class NXOpen.CAM.TrackpointBuilder

Bases: NXOpen.Builder

Represents a Trackpoint Builder

This is an abstract class and can not be instantiated

New in version NX5.0.0.

Properties

Property Description
Tag Returns the Tag for this object.
TlAdjReg Returns or sets the adjust register
TlCutcomReg Returns or sets the cutcom register
TrackingName Returns or sets the Tracking Point name value

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetObject Returns the object currently being edited by this builder.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

TlAdjReg

TrackpointBuilder.TlAdjReg

Returns or sets the adjust register

-------------------------------------

Getter Method

Signature TlAdjReg()

Returns:the tool adjust register
Return type:int

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature TlAdjReg(tlAdjReg)

Parameters:tlAdjReg (int) – The adjust register

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

TlCutcomReg

TrackpointBuilder.TlCutcomReg

Returns or sets the cutcom register

-------------------------------------

Getter Method

Signature TlCutcomReg()

Returns:the tool cutcom register
Return type:int

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

-------------------------------------

Setter Method

Signature TlCutcomReg(tlCutcomReg)

Parameters:tlCutcomReg (int) – The cutcom register

New in version NX5.0.0.

License requirements: cam_base (“CAM BASE”)

TrackingName

TrackpointBuilder.TrackingName

Returns or sets the Tracking Point name value

-------------------------------------

Getter Method

Signature TrackingName()

Returns:the tracking name value
Return type:str

New in version NX5.0.0.

License requirements: None.

-------------------------------------

Setter Method

Signature TrackingName(nameValue)

Parameters:nameValue (str) – the name value

New in version NX5.0.0.

License requirements: None.

Method Detail

Validate

TrackpointBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.