ToolPathTiltTiltingToolAxisTypes Enumeration

NXOpen.CAM.ToolPathTiltTilting.ToolAxisTypes is an alias for NXOpen.CAM.ToolPathTiltTiltingToolAxisTypes

class NXOpen.CAM.ToolPathTiltTiltingToolAxisTypes

Bases: object

the tool axis mode options

Enum Members

Enum Member Enum Member Description
TowardCurve
Tool axis mode: towards curve
FromCurve
Tool axis mode: from curve
TowardPoint
Tool axis mode: towards point
FromPoint
Tool axis mode: from point
RelativeAngle
Tool axis mode: relative MCS
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.