ToolPathTiltTiltingToolAxisTiltingDistTypes Enumeration

NXOpen.CAM.ToolPathTiltTilting.ToolAxisTiltingDistTypes is an alias for NXOpen.CAM.ToolPathTiltTiltingToolAxisTiltingDistTypes

class NXOpen.CAM.ToolPathTiltTiltingToolAxisTiltingDistTypes

Bases: object

the tool distance type options

Enum Members

Enum Member Enum Member Description
TwoD
Tool tilting distance type 2d
ThreeD
Tool tilting distance type 3d
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.