ToolPathSplitParametersBuilderTransferTypes Enumeration

NXOpen.CAM.ToolPathSplitParametersBuilder.TransferTypes is an alias for NXOpen.CAM.ToolPathSplitParametersBuilderTransferTypes

class NXOpen.CAM.ToolPathSplitParametersBuilderTransferTypes

Bases: object

Transfer type options

Enum Members

Enum Member Enum Member Description
Direct
direct transfer type
Clearance
clearance transfer type
LowestSafeZ
lowest safe z transfer type
Smooth
smooth transfer type
Plane
local plane transfer type
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.