ToolPathDivideBuilder Class¶
-
class
NXOpen.CAM.
ToolPathDivideBuilder
¶ Bases:
NXOpen.Builder
Represents a Tool Path Divide Builder
To create a new instance of this class, use
NXOpen.CAM.CAMSetup.CreateToolPathDivideBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ClearancePlane | Returns or sets the Clearance Plane tag,plane entity type covers Xform and Plane |
DistanceLimit | Returns or sets the time limit value |
DivideType | Returns or sets the divide limit type |
NumberOfDivideEvents | Returns the number of defined divide event indices |
Tag | Returns the Tag for this object. |
TimeLimit | Returns or sets the time limit value |
TolerancePercent | Returns or sets the time limit value |
UdeEndOfPath | Returns or sets the End of Path command |
UdeStartOfPath | Returns or sets the Start of Path command |
Methods¶
Method | Description |
---|---|
AddDivideEvent | Add a new divide event to the list |
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetAllDivideEvents | Returns all events where to of divide the tool path @return array with the divide event indices |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetDivideEvent | Gets the divide event at the given index @return the divide point |
GetObject | Returns the object currently being edited by this builder. |
RemoveAllDivideEvents | Delete all events where to of divide the tool path |
RemoveDivideEvent | Deletes the divide event at the given index |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ToolPathDivideBuilderPathDivideType Enumeration | Divide type options |
Property Detail¶
ClearancePlane¶
-
ToolPathDivideBuilder.
ClearancePlane
¶ Returns or sets the Clearance Plane tag,plane entity type covers Xform and Plane
-------------------------------------
Getter Method
Signature
ClearancePlane()
Returns: the clearance plane tag,entity type can be XFORM or PLANE Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ClearancePlane(clearancePlane)
Parameters: clearancePlane ( NXOpen.NXObject
) – the clearance plane tag,entity type can be XFORM or PLANENew in version NX5.0.0.
License requirements: None.
DistanceLimit¶
-
ToolPathDivideBuilder.
DistanceLimit
¶ Returns or sets the time limit value
-------------------------------------
Getter Method
Signature
DistanceLimit()
Returns: the distance_limit value Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DistanceLimit(distanceLimitValue)
Parameters: distanceLimitValue (float) – the distance limit value New in version NX5.0.0.
License requirements: None.
DivideType¶
-
ToolPathDivideBuilder.
DivideType
¶ Returns or sets the divide limit type
-------------------------------------
Getter Method
Signature
DivideType()
Returns: the divide type value Return type: NXOpen.CAM.ToolPathDivideBuilderPathDivideType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
DivideType(divideTypeValue)
Parameters: divideTypeValue ( NXOpen.CAM.ToolPathDivideBuilderPathDivideType
) – the divide_type valueNew in version NX5.0.0.
License requirements: None.
NumberOfDivideEvents¶
-
ToolPathDivideBuilder.
NumberOfDivideEvents
¶ Returns the number of defined divide event indices
-------------------------------------
Getter Method
Signature
NumberOfDivideEvents()
Returns: Return type: int New in version NX6.0.0.
License requirements: None.
TimeLimit¶
-
ToolPathDivideBuilder.
TimeLimit
¶ Returns or sets the time limit value
-------------------------------------
Getter Method
Signature
TimeLimit()
Returns: the time_limit value Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TimeLimit(timeLimitValue)
Parameters: timeLimitValue (float) – the time limit value New in version NX5.0.0.
License requirements: None.
TolerancePercent¶
-
ToolPathDivideBuilder.
TolerancePercent
¶ Returns or sets the time limit value
-------------------------------------
Getter Method
Signature
TolerancePercent()
Returns: the tolerance_percent value Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TolerancePercent(tolerancePercentValue)
Parameters: tolerancePercentValue (float) – the tolerance_percent value New in version NX5.0.0.
License requirements: None.
UdeEndOfPath¶
-
ToolPathDivideBuilder.
UdeEndOfPath
¶ Returns or sets the End of Path command
-------------------------------------
Getter Method
Signature
UdeEndOfPath()
Returns: the ude end of path Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UdeEndOfPath(udeEndOfPath)
Parameters: udeEndOfPath ( NXOpen.NXObject
) – the ude end of pathNew in version NX5.0.0.
License requirements: None.
UdeStartOfPath¶
-
ToolPathDivideBuilder.
UdeStartOfPath
¶ Returns or sets the Start of Path command
-------------------------------------
Getter Method
Signature
UdeStartOfPath()
Returns: the ude start of path Return type: NXOpen.NXObject
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UdeStartOfPath(udeStartOfPath)
Parameters: udeStartOfPath ( NXOpen.NXObject
) – the ude start of pathNew in version NX5.0.0.
License requirements: None.
Method Detail¶
AddDivideEvent¶
-
ToolPathDivideBuilder.
AddDivideEvent
¶ Add a new divide event to the list
Signature
AddDivideEvent(divideEvent)
Parameters: divideEvent (int) – index of the new divide event New in version NX6.0.0.
License requirements: None.
GetAllDivideEvents¶
-
ToolPathDivideBuilder.
GetAllDivideEvents
¶ Returns all events where to of divide the tool path
Signature
GetAllDivideEvents()
Returns: array with the divide event indices Return type: list of int New in version NX6.0.0.
License requirements: None.
GetDivideEvent¶
-
ToolPathDivideBuilder.
GetDivideEvent
¶ Gets the divide event at the given index
Signature
GetDivideEvent(index)
Parameters: index (int) – position of the event to get Returns: the divide point Return type: int New in version NX6.0.0.
License requirements: None.
RemoveAllDivideEvents¶
-
ToolPathDivideBuilder.
RemoveAllDivideEvents
¶ Delete all events where to of divide the tool path
Signature
RemoveAllDivideEvents()
New in version NX6.0.0.
License requirements: None.
RemoveDivideEvent¶
-
ToolPathDivideBuilder.
RemoveDivideEvent
¶ Deletes the divide event at the given index
Signature
RemoveDivideEvent(divideEvent)
Parameters: divideEvent (int) – the index to delete New in version NX6.0.0.
License requirements: None.
Validate¶
-
ToolPathDivideBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.