ToolAxisTiltTypes Enumeration¶
NXOpen.CAM.ToolAxisTilt.Types is an alias for NXOpen.CAM.ToolAxisTiltTypes
-
class
NXOpen.CAM.
ToolAxisTiltTypes
¶ Bases:
object
Available types for tool axis tilt control
Enum Members
Enum Member Enum Member Description NotSet No tiltingAwayFromPart Tilt away from partAwayFromPoint Tilt away from pointTowardPoint Tilt tpward pointAwayFromCurve Tilt away from curveTowardCurve Tilt toward curve-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-