ToolAxisTiltTiltAngleTypes Enumeration

NXOpen.CAM.ToolAxisTilt.TiltAngleTypes is an alias for NXOpen.CAM.ToolAxisTiltTiltAngleTypes

class NXOpen.CAM.ToolAxisTiltTiltAngleTypes

Bases: object

Available types for auto tilt

Enum Members

Enum Member Enum Member Description
Automatic
Automatically calculate tilt angle
Specify
User specifies the tilt angle
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.