ToolAxisAdvancedType Enumeration

NXOpen.CAM.ToolAxisAdvanced.Type is an alias for NXOpen.CAM.ToolAxisAdvancedType

class NXOpen.CAM.ToolAxisAdvancedType

Bases: object

Available types for Tool Axis Advanced type

Enum Members

Enum Member Enum Member Description
Automatic
Automatic
InterpolateVector
Interpolate Vector
BladeSwarf
Blade Swarf
FollowBladeUv
Follow Blade UV
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.