ThreadedHoleSet Class¶
-
class
NXOpen.CAM.
ThreadedHoleSet
¶ Bases:
NXOpen.CAM.HoleBossSet
Represents a Cut Area Geometry builder
To create a new instance of this class, use
NXOpen.CAM.HoleBossGeom.CreateThreadedHoleBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Depth | Returns or sets the Depth |
DepthBuilder | Returns the depth builder |
DepthLimit | Returns or sets the Depth Limit types |
Diameter | Returns or sets the Diameter |
DiameterBuilder | Returns the diameter builder |
Length | Returns or sets the Length |
LengthBuilder | Returns the length builder |
MajorDiameter | Returns or sets the Major Diameter |
MinorDiameter | Returns or sets the Minor Diameter |
RadialEngage | Returns or sets the Radial Engage |
Size | Returns or sets the Size |
StartDiameter | Returns the start diameter |
Tag | Returns the Tag for this object. |
TapDrillSize | Returns or sets the Tap Drill Size |
TapDrillSizeBuilder | Returns the Tap Drill Size builder |
TipAngle | Returns the tip angle |
ToolAxis | Returns or sets the Tool Axis |
Methods¶
Method | Description |
---|---|
GetFeature | Returns the in process feature @return |
GetMachiningFeature | Returns the machining feature @return |
GetStandard | The Standard @return the Standard |
InferLogic | Save the infer logic information of the input entity, such as the orientation, pitch, diameter and height etc. |
ReverseDirection | Reverses the direction of the feature |
SetStandard | The Standard |
Property Detail¶
RadialEngage¶
-
ThreadedHoleSet.
RadialEngage
¶ Returns or sets the Radial Engage
-------------------------------------
Getter Method
Signature
RadialEngage()
Returns: the Radial Engage Return type: str New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
RadialEngage(threadHoleValue)
Parameters: threadHoleValue (str) – the Radial Engage New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TapDrillSize¶
-
ThreadedHoleSet.
TapDrillSize
¶ Returns or sets the Tap Drill Size
-------------------------------------
Getter Method
Signature
TapDrillSize()
Returns: Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TapDrillSize(doubleValue)
Parameters: doubleValue (float) – New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
TapDrillSizeBuilder¶
-
ThreadedHoleSet.
TapDrillSizeBuilder
¶ Returns the Tap Drill Size builder
-------------------------------------
Getter Method
Signature
TapDrillSizeBuilder()
Returns: Return type: NXOpen.CAM.InferredDouble
New in version NX7.5.0.
License requirements: None.