ThreadedBossSet Class¶
-
class
NXOpen.CAM.
ThreadedBossSet
¶ Bases:
NXOpen.CAM.HoleBossSet
Represents a thread boss Geometry builder
To create a new instance of this class, use
NXOpen.CAM.HoleBossGeom.CreateThreadedBossBuilder()
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
Depth | Returns or sets the Depth |
DepthBuilder | Returns the depth builder |
DepthLimit | Returns or sets the Depth Limit types |
Diameter | Returns or sets the Diameter |
DiameterBuilder | Returns the diameter builder |
Height | Returns or sets the Height |
Length | Returns or sets the Length |
LengthBuilder | Returns the length builder |
MajorDiameter | Returns or sets the Major Diameter |
MinorDiameter | Returns or sets the Minor Diameter |
Size | Returns or sets the Size |
StartDiameter | Returns the start diameter |
Tag | Returns the Tag for this object. |
TipAngle | Returns the tip angle |
ToolAxis | Returns or sets the Tool Axis |
Methods¶
Method | Description |
---|---|
GetFeature | Returns the in process feature @return |
GetMachiningFeature | Returns the machining feature @return |
InferLogic | Save the infer logic information of the input entity, such as the orientation, pitch, diameter and height etc. |
ReverseDirection | Reverses the direction of the feature |
Property Detail¶
Height¶
-
ThreadedBossSet.
Height
¶ Returns or sets the Height
-------------------------------------
Getter Method
Signature
Height()
Returns: the Height Return type: float New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Height(holeBossValue)
Parameters: holeBossValue (float) – the height New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)