ThreadTurningBuilderInfeedLengthTypes Enumeration

NXOpen.CAM.ThreadTurningBuilder.InfeedLengthTypes is an alias for NXOpen.CAM.ThreadTurningBuilderInfeedLengthTypes

class NXOpen.CAM.ThreadTurningBuilderInfeedLengthTypes

Bases: object

the Infeed Length Types

Enum Members

Enum Member Enum Member Description
Auto
Auto
Specify
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.