ThreadToolBuilderInsertShapes Enumeration

NXOpen.CAM.ThreadToolBuilder.InsertShapes is an alias for NXOpen.CAM.ThreadToolBuilderInsertShapes

class NXOpen.CAM.ThreadToolBuilderInsertShapes

Bases: object

the available insert shapes

Enum Members

Enum Member Enum Member Description
Standard
Standard insert shape
Trapezoidal
Trapezoidal insert shape
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.