TeachmodeProfileMoveBuilderStartStopPositionMethods Enumeration

NXOpen.CAM.TeachmodeProfileMoveBuilder.StartStopPositionMethods is an alias for NXOpen.CAM.TeachmodeProfileMoveBuilderStartStopPositionMethods

class NXOpen.CAM.TeachmodeProfileMoveBuilderStartStopPositionMethods

Bases: object

the start and stop positioning methods

Enum Members

Enum Member Enum Member Description
Drive
Use drive geometry start or stop point
Point
Use selected point
Check
Use selected check geometry
ContourPosition
Use end point of last contouring
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.