TeachmodeProfileMoveBuilderDriveGeometryTypes Enumeration

NXOpen.CAM.TeachmodeProfileMoveBuilder.DriveGeometryTypes is an alias for NXOpen.CAM.TeachmodeProfileMoveBuilderDriveGeometryTypes

class NXOpen.CAM.TeachmodeProfileMoveBuilderDriveGeometryTypes

Bases: object

the drive geometry types

Enum Members

Enum Member Enum Member Description
PreviousCheck
Use Previous Drive Geometry
PreviousDrive
Use Previous Stop Check Geometry
NewDrive
Use New Drive Geometry
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.