TabPointDataBuilderTabMethodType Enumeration

NXOpen.CAM.TabPointDataBuilder.TabMethodType is an alias for NXOpen.CAM.TabPointDataBuilderTabMethodType

class NXOpen.CAM.TabPointDataBuilderTabMethodType

Bases: object

Tab Point Method Options

Enum Members

Enum Member Enum Member Description
StartAndEndPoint
Start and End point
PointAndWidth
Point and Width
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.