SurfaceContourBuilderDriveMethodTypes Enumeration

NXOpen.CAM.SurfaceContourBuilder.DriveMethodTypes is an alias for NXOpen.CAM.SurfaceContourBuilderDriveMethodTypes

class NXOpen.CAM.SurfaceContourBuilderDriveMethodTypes

Bases: object

Available types for Drive Method

Enum Members

Enum Member Enum Member Description
Undef
Undefined
Curve
Curve/Point
Spiral
Spiral
Boundary
Boundary
AreaMilling
Area Milling
SurfaceArea
Surface Area
InterpolatedToolPath
Interpolated tool path
ToolPath
Tool Path
RadialCut
Radial Cut
ContourProfile
Contour Profile
FlowCut
Flow Cut
Text
Text
UserDefined
User Function
BladeRough
Blade Rough
BladeFinish
Blade Finish
HubFinish
Hub Finish
BlendFinish
Blend Finish
EdgeFinish
Edge Finish
RotaryFloorFinish
Rotary Floor Finish
Total
Total
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.