StopPosition Class¶
-
class
NXOpen.CAM.
StopPosition
¶ Bases:
NXOpen.TaggedObject
Represents a stop position
New in version NX6.0.0.
Properties¶
Property | Description |
---|---|
Distance | Returns or sets the stop at distance |
Percentage | Returns or sets the stop at percentage |
Point | Returns or sets the stop at point |
Tag | Returns the Tag for this object. |
Type | Returns or sets the stop at mode |
Methods¶
Enumerations¶
StopPositionTypes Enumeration | the stop at options |
Property Detail¶
Distance¶
-
StopPosition.
Distance
¶ Returns or sets the stop at distance
-------------------------------------
Getter Method
Signature
Distance()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Distance(stopAtDistance)
Parameters: stopAtDistance (float) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Percentage¶
-
StopPosition.
Percentage
¶ Returns or sets the stop at percentage
-------------------------------------
Getter Method
Signature
Percentage()
Returns: Return type: float New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Percentage(stopAtPercentage)
Parameters: stopAtPercentage (float) – New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Point¶
-
StopPosition.
Point
¶ Returns or sets the stop at point
-------------------------------------
Getter Method
Signature
Point()
Returns: the stop at point Return type: NXOpen.Point
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Point(stopAtPoint)
Parameters: stopAtPoint ( NXOpen.Point
) – the stop at pointNew in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)
Type¶
-
StopPosition.
Type
¶ Returns or sets the stop at mode
-------------------------------------
Getter Method
Signature
Type()
Returns: Return type: NXOpen.CAM.StopPositionTypes
New in version NX6.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Type(stopAtMode)
Parameters: stopAtMode ( NXOpen.CAM.StopPositionTypes
) –New in version NX6.0.0.
License requirements: cam_base (“CAM BASE”)