StepoverBuilderApplyTypes Enumeration

NXOpen.CAM.StepoverBuilder.ApplyTypes is an alias for NXOpen.CAM.StepoverBuilderApplyTypes

class NXOpen.CAM.StepoverBuilderApplyTypes

Bases: object

apply on part options

New in version NX6.0.0.

Enum Members

Enum Member Enum Member Description
OnPlane
Apply on Plane
OnPart
Apply on Part
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.